Press
 

Press Release

 

Mobility

Siemens receives funding approval for developing fuel cell drive for trains

Feb 26, 2018, Munich

  • Siemens and Ballard jointly develop fuel cell drive for trains
  • German Federal Ministry for Transportation and Digital Infrastructure funds project with around €12 million
  • Mireo regional and commuter train platform to be reference
  • Zero-emission operation without overhead lines

Siemens and Ballard Power Systems Inc., a Canadian manufacturer of fuel cells, plan the joint development of a fuel cell drive for the Siemens Mireo train platform. Working together, the two companies intend to develop a new generation of fuel cells with an especially long lifecycle and high power density as well as improved efficiency. RWTH Aachen University is a partner in the research project. The German Federal Ministry for Transportation and Digital Infrastructure (BMVI) will support Siemens and RWTH Aachen with project funding of roughly €12 million as part of the Ministry's "National Hydrogen and Fuel Cell Technology Innovation Program". The program will be coordinated by the National Organization for Hydrogen and Fuel Cell Technology (NOW GmbH).

"We are seeing a rapid rise in demand for CO2-free fuel cell technology. This applies to all sectors of passenger and freight transport, whether it is trains, trams, buses or trucks," says Randy MacEwen, President and CEO of Ballard Power Systems.

"Our cooperation with Ballard marks a decisive step being taken to replace diesel-powered rail vehicles with emission-free vehicles in order to provide sustainable and climate-friendly mobility over the long term. We want to be able to offer our customers flexible train solutions – that vary depending on regional conditions and technical possibilities – for different types of local rail routes," says Sabrina Soussan, CEO of the Siemens Mobility Division.

The long-term goal of the cooperation is to develop a modular and scalable traction system with fuel cells that will be integrated into the Mireo train platform. With such a system, the Mireo can flexibly operate in various ways – battery-electric as well as on routes without overhead lines – with the help of hydrogen-fueled trains. The fuel cell technology is to be ready for service by 2021, and its integration in additional vehicle platforms will follow.

The new Mireo regional and commuter platform from Siemens was specially developed for sustainable and flexible operations, and is thus predestined for the testing of an alternative drive system. Thanks to its lightweight construction, energy-efficient components and intelligent electrical system management, the Mireo uses up to 25 percent less energy compared to trains with similar passenger capacity.

Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active around the globe, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2017, which ended on September 30, 2017, Siemens generated revenue of €83.0 billion and net income of €6.2 billion. At the end of September 2017, the company had around 377,000 employees worldwide. Further information is available on the Internet at www.siemens.com.

Mrs. Eva Haupenthal
+49 (89) 636-24421
Share this site via